StateEntryShut
Syntax
<Path>.StateEntryShut:boolean |
The attribute StateEntryShut sets the state of the Frame to entrance closed (true) or not closed (false). The Frame only shows this state if the Recovery time is active. Then, the Frame shows a light blue dot in the LED area of the icon.
Data Type of the Value You Can Assign
You can assign a value of data type boolean.
Example
Frame.StateEntryShut := true |
Related Topic
Related Topics
Attributes of the FrameAxesOrigin
BackgroundColor (Frame)
Failed (Frame)
ModifyStructure
Pause (Frame)
ReplacementMode
RepresentationMode
RotateMUs (Frame)
ScalingFactor
ShiftCalendarObject (Frame)
ShowDisplayPanels
ShowObjectLabels
ShowObjectNames
StateBlocked
StateResourceMissing
StateSetup
StateWorking
Unplanned (Frame)
ZoomFactor