InitValue
Syntax
&Variable.InitValue:any |
The attribute InitValue resets a value, which the Variable recorded during a simulation run, to an initial value during the init phase of the next simulation run.
Note:
The Data types table, list, stack, queue, and randtime do not provide this feature.
Data Type of the Value You Can Assign
You can assign a value of data type any.
Example
&MyVariable.InitValue := 0 |
Related Topic