Information Flow Objects
Tecnomatix Plant Simulation provides these objects for providing the simulation with information during the simulation runs:
The Method for programming controls and the Variable for storing data over an extended period of time.
The lists and tables DataList , DataQueue DataStack , DataTable , and TimeSequence .
The Trigger and the Generator for controlling when and how mobile objects (MUs) are created.
The AttributeExplorer for managing the attributes defining the settings of the individual stations in your simulation model.
The FileInterface for exchanging data with other applications.
The FileLink for exchanging data with other applications.
The XMLInterface for exchanging data with other applications.
Note that the Inter-Process Communication Interfaces and the Database Interfaces are also part of the information flow objects.
We renamed the following objects in Plant Simulation 14.1 and 14.2:
Up to Version 14.0 | From Version 14.1 on |
---|---|
Assembly | AssemblyStation |
Line | Conveyor |
ParallelProc | ParallelStation |
SingleProc | Station |
Entity | Part |
Up to Version 14.1 | From Version 14.2 on |
---|---|
TableFile | DataTable |
CardFile | DataList |
StackFile | DataStack |
QueueFile | DataQueue |
As we created some of the models for the Online Help in previous versions, some of the screenshots still show the previous names of the objects.
Related Topic