CursorY
Syntax
<Path>.CursorY |
The attribute CursorY sets the row in which the internal cursor is located. The method find starts searching from the current cursor position and sets the cursor to the next found item. The methods max and min set the cursor to the maximum or minimum value of the given range. Plant Simulation ignores ranges located before the current cursor position. The Method starts its task beginning at the cursor position. If a Method does not return the expected values, check the cursor position. The first column has the number 1. If you also want to include the user-defined index, set the attribute CursorY to 0.
This attribute applies to the DataTable and the TimeSequence.
Data Type of the Value You Can Assign
You can assign a value of data type integer.
Example
MyDataTable.CursorX := 1 -- starting position |
You can also set the pointer by employing a user-defined index. For a user-defined index of data type integer, use the method setCursor!
Example
MyDataTable.CursorY := "urgent" -- user-defined index |
Related Topics
Related Topics
Attributes of the DataTableChanged
ColumnIndex
CursorX
DataType (DataTable)
DataTypeColumnIndex
FastAccessColumnIndex
FastAccessRowIndex
FormatString (DataTable)
FormatStringColumnIndex
FormatStringRowIndex
MaxXDim
MaxYDim
Name (DataTable)
RowIndex
ShowColumnIndex (DataTable)
ShowRowIndex (DataTable)
UniqueKeyColumnIndex
UniqueKeyRowIndex