Item
Syntax
<Path>.Item:string |
The attribute Item sets which item in the Drop-Down List designated by <Path> will be selected using its name.
Note:
If you localize the items, you will usually use the attribute Value instead of the attribute Item. The value is a number which is language-independent, while the Item is a string which differs from language to language.
Data Type of the Value You Can Assign
You can assign a value of data type string.
Example
MyDropdownList.Item := "My item text 1" |
Related Topics
Items, dialog element
Items, attribute