DisplayType
Syntax
<Path>.DisplayType:string |
The attribute DisplayType sets if the Display shows the input value as text, as a bar, or as a pie segment. Bar and pie representation map values in a specified range to bars of varying heights or pies with a varying degree of completion. You can set the range with the attributes MinVal and MaxVal.
Data Type of the Value You Can Assign
You can assign a value of data type string: Text, Bar, or Pie.
Example
MyDisplay.DisplayMode := "Text" |
Related Topic