LabelFont
Syntax
<Path>.LabelFont:string |
The attribute LabelFont and its sub-attribute set the properties of the Labels of the axes in the Chart window.
Data Type of the Value You Can Assign
You can assign a value of data type string.
You can enter one of these fonts:
Arial |
Arial Narrow |
Comic Sans MS |
Courier New |
Haettenschweiler |
Lucida Console |
MS UI Gothic |
Tahoma |
Times New Roman |
Trebuchet MS |
Verdana |
MS UI Gothic is intended for our Japanese users. An English or a German version of Microsoft Windows might not provide this font by default.
Example
MyChart.LabelFont:= "Tahoma" |
The sub-attribute Size, of data type integer, sets the font Size. You can enter a number between 1 and 8.
Example
MyChart.LabelFont.Size := 4 |
The numbers in the drop-down list are not actual point sizes, but set a factor the Chart uses for sizing labels.
The sub-attribute Bold, of data type boolean, sets if the Chart shows the labels in bold face (true or not (false).
Example
MyChart.LabelFont.Bold := true |
The sub-attribute Italic, of data type boolean, sets if the Chart shows the labels in italics (true) or not (false).
Example
MyChart.LabelFont.Italic := false |
Related Topic
Related Topics
Attributes of the ChartAccumulated
Active (Chart)
Category
ChartType
CollectData (Chart)
DataInColumn
DataRange
DataTable (Chart)
DisplayInFrame
Effect
FeedRate
FirstInterval
GapWhenNull
GraphTable
Height (3D charts)
ImageQuality3D
InputChannels
LegendLocation
Mode (Chart)
NullValue
NumIntervals
NumValues
Rotation (Chart)
SampleInterval
Scrollbar
SizeInFrame
StepCurve
StepSize
Subtitle
SubtitleFont
TableFont
Title
TitleFont
UseInputChannels
UseMetricPrefix
XGrid
XGridlines
XLabel
XRange
XScaleMax
XScaleMin
XLog
YGrid
YGridLineInterval
YLabel
YLog
YScaleMax
YScaleMin
ZLabel