BayDepth
Syntax
<Path>.BayDepth:length |
The attribute BayDepth sets the depth of a single storage bay of the rack designated by <Path>.
Note:
When you assign the attribute, Plant Simulation deactivates graphic inheritance.
Note:
You cannot assign the attribute when the graphic is an automatically generated graphic group or when the graphic is located in an automatically generated graphic group.
Note:
The attribute BayDepth indirectly also sets the depth of the entire rack.
Data Type of the Value You Can Assign
You can assign an array of data type length.
Example
MyFrame._3D.getGraphic("deco", [8]).BayDepth := 1.5 |
Related Topics
Rack > Rack Settings