Manage the status of a study using Study Manager
Add a status to the study
Locate a study using the Study Manager dialog box.
In the Study Manager dialog box, select one or multiple studies.
Click Set Status → Approved.
Status is added to the study object.
View the status of a study
Locate a study using the Study Manager dialog box.
In the Study Manager dialog box, choose Table Columns → Select Columns.
The Columns Selector dialog box is shown.
In the Columns Selector dialog box, type stat in the Available Fields box.
In the Columns Selector dialog box, select Release Status in the list of available fields, click Add , and click OK.
The Release Status column is added to the table.
Remove a status from the study
Locate a study using the Study Manager dialog box.
In the Study Manager dialog box, select one or multiple studies.
Click Set Status → Remove Approve State.
Status is removed from the study object.