Study Manager for fixture planning
Teamcenter Manufacturing Access is developed on top of the Active Workspace platform and is the technology behind the NX Fixture Planner Study Manager tab of the resource bar. This tab enables fixture planners to perform more of their tasks within NX and reduces the dependency on the Teamcenter rich client.
Using the Study Manager tab of the resource bar, fixture planners can do the following:
Search for a collaboration context, and view a list of its studies.
Set the project on which you are currently working, so you can see the project's related collaboration contexts and studies.
Create a study.
Edit study contents.
Load a study into NX.
Fixture Planner is an application within Teamcenter Integration for NX that you can use to design and manage the stations and other components using resources stored in Teamcenter. For more information see the NX Fixture Planner documentation.