Assignment status icons
When you assign operations from the product BOP to the plant BOP, Production Process Planning uses special icons to indicate the assignment status if the Show indication information mode is active. These indications are based on the line balancing scope. For example, if you are viewing a zone with 10 stations, the line balancing scope is the zone.
(Blank) Unassigned to any process area. | |
The operation is assigned to a process area in the current line balancing scope. Click the icon to jump to the process area in the current scope and highlight the operation in the Operations list. | |
The operation is assigned to a process area that is not in the current line balancing scope. | |
The operation is assigned to multiple process areas, including areas in the current line balancing scope and possibly in another scope. Click the icon to see a list of the process areas where the operation is assigned. In the example below, the operation is located in three process areas in the current scope and three in a different scope. | |
The operation is assigned to multiple process areas. However, none of them are in the current line balancing scope. | |
The operation has properties that were changed in the current scope of the plant BOP or the product BOP after allocation. This is a in-scope partial match warning. | |
The operation has properties that were changed in another scope of the plant BOP or the product BOP after allocation. This is a out-of-scope partial match warning. | |
The operation was deleted from the product BOP after it was allocated to the plant BOP. This is a missing in source error. |