View process area planning
In the plant BOP, process area planning is performed on the process station and process area pages. This includes the process stations, the process resources, and the operations to be performed in the process area.
Process areas
The plant BOP contains a hierarchy of process areas, such as process lines, process areas, or process station objects. The lowest level of this hierarchy is the process station where the work is performed.
(Optional) Process resource
A process resource object is used to group operations in a station that are assigned to a specific active resource, such as a worker or robot. For example, Station 10 could contain these two process resources: Left side worker and Right side worker.
Operation
Each process station object contains operations that describe the high-level tasks to perform. Operations can be sequenced. For example, the Station 10 process station could contain this operation: Add Instrument Panel.