Edit basic BOM line properties
This feature allows you to edit basic properties for a bill of materials (BOM) line and its associated objects.
Note:
To use this feature, you must be running Teamcenter Active Workspace 4.1.1 or later and your Teamcenter administrator must also install the EasyPlan Active Workspace Infrastructure using the Teamcenter Environment Manager.
Navigate to your plant BOP.
Open the process line, process station, or operation that you want to edit, and click the Details tab.
Click Start Edit .
Note:If the object is released, a message displays to suggest that you revise the object before you start editing.
Modify properties associated with the object as needed.
Save or cancel your edits.