Assign resources to an operation
During process planning, you must assign the resources used during an operation to create parts. You assign resources to an operation in the plant bill of process (BOP) structure.
Navigate to a process area or process line that contains process stations.
Open a process station.
On the Planning tab, under the Resources subtab, navigate to display the resources you want to assign.
In the Operations table, select the target operation.
Select and drag from the Resources subtab to the Assigned Resources tab for the selected operation.
(Optional) To remove a resource from an operation, select the resource in the Assigned Resources tab, and click Unassign .