View operation planning
In the plant BOP, operation planning is performed on the operation page. This includes the activities, parts, and tools that are needed to perform the operation.
Operation
Each process station object contains operations that describe the high-level tasks to be performed. Operations can be sequenced. For example, the Station 10 process station could contain this operation: Add Instrument Panel.
Time
Each operation contains time objects that describe the more detailed tasks to be performed in the operation and can be sequenced. For example, you could create these activities to describe how to insert an instrument panel into a car: Maneuver Lift Assist Holding Instrument Panel through Car Door, Secure Instrument Panel to Car, and Remove Empty Lift Assist from Car.
Parts
These are the parts associated to the operation.
Tools
These are the tool associated to the operation.
Documents
Reference documents can be added to operations and activities.