Edit operation frequency
You can edit operation frequency to produce a more accurate operation time.
Note:
In the Operation Frequency field, the left number in the fraction is the Repeats value and the right number is the Per Cycle value. To calculate the total operation time, you multiply this fraction by the sum of the activities. For example, if the sum of the activities is 2, and the frequency is 1 repeat per 2 cycles (1/2), the operation total time is 2 * (1/2) = 1.
Click the Time tab.
In the summary row at the bottom of the table, click Edit Operation Frequency .
Type in new values for the operation frequency.