Manage station comments during line balancing
During line balancing, you can use the comments feature to add notes about changes you make. This helps you track planning changes and avoid confusion when multiple planners work within the same structure.
If a station contains comments, the station displays a comment bubble. Hover over the comment bubble to review the comments.
Add or edit a comment
Use these steps to add or edit comments to a station.
In the plant bill of process (BOP), navigate to a process area or process line and click the Balancing tab.
Select a station tile, click More , and select Add Comment.
Type text in the Add Comment dialog box, and click Done.
Note:If a station is released, a message displays stating that the object must be revised to complete the action. If you add, edit, or delete a comment, that is considered a revision to the station.
Click Yes, Revise.
Delete a comment
Use these steps to delete an existing comment from a station.
In the plant BOP, navigate to a process area or process line and click the Balancing tab.
Select a station tile, click More , and select Edit Comment.
Click Delete comment for this station.
The comment permanently disappears from the station.
Note:If a station is released, a message displays stating that the object must be revised to complete the action. If you add, edit, or delete a comment, that is considered a revision to the station.
Click Yes, Revise.