Register Easy Plan workspaces
After you install or update Easy Plan, you must register each workspace to a group or role in the Teamcenter organization.
This procedure is not required for Teamcenter Manufacturing Access.
Create a new file using a text editor that reads XML files, such as Notepad++.
Type the following content in the XML file:
<?xml version="1.0" encoding="UTF-8" standalone="no" ?>
<Import>
<Workspace id="workspace name">
<WorkspaceMapping role="TC organization role" group="TC organization role" default="true"/>
</Workspace>
</Import>
Edit the Workspace id and type in a value for the workspace name:
IEWorkspace to register Production Process Planning.
WIWorkspace to register Work Instructions Authoring.
Edit the WorkspaceMapping role to register the workspace for a group or a role.
Note:You can also register the workspace to both the group and role.
Open the Teamcenter command line, and run the following command:
import_wsconfig -u=TC admin user -p=TC admin password -g=dba -file=full XML file path
See Sample XML file for an example file used to register Easy Plan workspaces.